Public Enum Status Inherits System.Enum
public enum Status : System.Enum
public enum class Status : public System.Enum
Member | Description |
---|---|
AccessDenied | Insufficient permissions for operation. |
AlarmArchiverUnavailable | Alarm and Event subsystem unreachable. |
ArgumentException | A supplied argument is invalid. |
ArgumentNullException | A supplied argument is NULL. |
ArgumentOutOfRangeException | A supplied argument is outside the valid range. |
BackupInsufficientSpace | Insufficient disk space to perform backup. |
CircularReference | Circular reference detected in calculation. |
CollectorNotFound | The given collector does not exist on the server. |
DeleteOutsideActiveRange | Attempted data delete outside allowed modification interval. |
DuplicateCollector | The given collector name already exists on the server. |
DuplicateData | Attempt to overwrite an existing data sample. |
Failed | Operation failed. |
InternalLicenseError | Internal license error. |
InvalidCustomDataType | The Custom data type is not supported. |
InvalidDataStore | The requested data store was not found. |
InvalidEnumeratedSet | The requested Enumerated Set was not found. |
InvalidServerVersion | Operation unsupported due to server version. |
InvalidTagname | The requested tag was not found. |
InvalidUsername | Bad user name or password. |
LicensedConnectionCountExceeded | Number of licensed server connections exceeded. |
LicensedTagCountExceeded | Number of licensed tags exceeded. |
NotConnected | Not connected to Historian server. |
NotLicensed | Server or feature is not licensed. |
NotPermitted | Operation not permitted. |
NotSupported | Operation not supported. |
NoValue | No available tag data. |
QueryResultSizeExceeded | Upper limit on query results exceeded. |
Success | Operation successful. |
Timeout | Operation failed due to timeout. |
WriteArchiveOffline | Attempted data write to an offline archive. |
WriteArchiveReadonly | Attempted data write to a read-only archive. |
WriteInFuture | Attempted data write too far in the future. |
WriteNoArchiveAvailable | Attempted data write with no available archives. |
WriteOutsideActiveRange | Attempted data write beyond the configured active range. |
System.Object
System.ValueType
System.Enum
Proficy.Historian.ClientAccess.API.Status
Target Platforms: Windows 98, Windows NT 4.0, Windows Millennium Edition, Windows XP Home Edition, Windows XP Professional, Windows Server 2003 family, Windows Vista, Windows Server 2008 family