Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / EnumeratedSetStateName Class
Members


EnumeratedSetStateName Class
Represents details of an Enumerated Set State Name.
Syntax
Public Class EnumeratedSetStateName 
Inheritance Hierarchy

System.Object
   Proficy.Historian.ClientAccess.API.EnumeratedSetStateName

Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also