Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / EnumeratedSetState Class
Members


EnumeratedSetState Class
Represents details of an Enumerated Set State.
Syntax
Public Class EnumeratedSetState 
Inheritance Hierarchy

System.Object
   Proficy.Historian.ClientAccess.API.EnumeratedSetState

Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also