Install the Historian Excel Add-in Using the Installer
Before you begin
- Microsoft® Excel® 2024 (32 & 64 bit)
- Microsoft® Excel® 2021 (32 & 64 bit)
- Microsoft® Excel® 2019 (32 & 64 bit)
- Microsoft® Excel® 2016 (32 & 64 bit)
About this task
Procedure
- Mount the ISO.
-
From the mounted ISO, run the InstallLauncher.exe
file.
The Proficy Historian Installation page appears.
-
Select Install Excel Add-in for Historian.
The installer runs through the installation steps.Note:If using certain versions of Windows (like Windows 10 or Windows 2019), you may receive an error message, stating that some of the DLL files are not registered. You can ignore these messages.
- When prompted to reboot your system, select Yes.