Generating a Request File

Generate a request file from an offline computer.

Procedure

  1. From the License Client, click the Activate Licenses tab.
    The License Client detects that the client computer is not connected to the Internet. The "Do you need to activate a License?" page appears.
  2. Click Yes, for a permanently offline computer.
    The Generate a Request File to activate licenses page appears.


  3. Browse to the media device or network location where the request file will be saved.
  4. Enter each activation code and click Add Code to add it to the Activation Codes area.
    Note:
    The activation codes can be found in the email you received from GE Vernova.
  5. Click Generate File to create and save a request file to the specified location.
    The Complete Offline Process page appears. A message indicates the request file location and when it was created.


What to do next

  • If you are using a portable media device, remove it and go to the online computer. Leave the License Client application running.
  • Generate a response file from the offline client computer.