Generating a Response File

Generate a response file from an online computer.

Before you begin

  • Start the License Client.
  • Verify that License Server has been selected as the license activation mechanism and that the Connection Status is Online in Advanced Operations.

Procedure

  1. Click Complete Offline Process.
    The Complete Offline Process page appears. A message indicates the response file location and when it expires.
  2. Click Generate a response file from an online computer.

    The Generate a Response File page appears.



  3. If necessary, insert the media device into the computer.
  4. Select the request filesand the response folder location, then click Generate File.

    The response file is generated and saved to the specified location on a media device or network drive that can be accessed by the offline computer.



    Note:
    The response file expires 24 hours after being created. The application indicates how much time is remaining before the response file expires.

What to do next

If you are using a portable media device to store the response file, remove it and return to the offline computer.