Plant Applications Client
The Plant Applications Client provides a customizable environment for using Plant Applications Views and Displays to access your plant data. For more information about using the Plant Applications Client, refer to Plant Applications Help.

Legend:
- A View is a group of displays that can be opened at the same time. Views are created in the Plant Applications Client.
- The toolbar provides a quick way to perform tasks specific to the active display. The toolbar automatically changes depending on which display is active.
- The box indicates the status of the connection to the Plant Applications Server. Green indicates the connection is active.
- This area displays the name of the person who is currently logged in to the Plant Applications Client.
- Click the tabs to switch between displays.