Standard Edition Web Client Requirements

Before you begin

Review the following preinstallation requirements before you run the Plant Applications Web Client installer:

System Requirements

Ensure that your computer meets the system requirements as described in the following table. For more information, refer to the System Requirements section in the Plant Applications Getting Started Guide document for the latest Plant Applications release.

The Plant Application Server and Web Client servers can be hosted in the AWS/Azure Cloud. Ensure that when they are hosted in Cloud they meet the Plant Application and Web Client Server system requirements.

Item Version
Operating system 64-bit Windows 10 or Windows Server 2022
Couch DB server CouchDB version 2.3.1 or 3.2.2
Note:
For more information on downloading, installing, configuring, or upgrading CouchDB, refer to the Pre-installation Configuration (Enterprise and Standard) section.
Operations Hub 2.1 with SIM3 and later, or Operations Hub 2022, 2022.4.1, or 2022.06
Web browsers Chrome 107.0.5304.107 and later

Devices:

  • iPad: Safari v13.1+, Chrome 107.0.5304.107 and later
    Note:
    To view the application content, you must select the desktop site option from the Chrome browser settings menu.
  • Windows Tablet: Chrome 107.0.5304.107 and later
    Note:
    Devices support only Unit Operations,Work Queue, and Non Conformance applications.
  • Android 10-inch Tablet: Chrome 107.0.5304.107 and later.
    Note:
    To view the application content, you must select the desktop site option from the Chrome browser settings menu.

Microsoft Edge v94.0.992.31

OLEDB Driver Microsoft OLE DB Driver 18 for SQL Server
Note:
You can download the Microsoft OLE DB Driver 18 for SQL Server from the following URL: https://www.microsoft.com/en-us/download/details.aspx?id=56730.
Hard drive 100 GB (minimum recommended)
Processor 2.4 GHz clock-speed Intel Core i3, i5, or i7 CPU or equivalent AMD Phenom CPU
Note:
For better performance, we recommend to use a 16 core processor.
Memory 32 GB (minimum recommended)
Note:
You must have minimum 64 GB or more if you plan to install Web Client, Historian, Operations Hub, and Plant Applications on the same node. However, it is recommended to install them in a distributed environment.

Port Requirements

This section describes the port requirements for Plant Applications Web Client. Ensure that the ports described in the following table are opened before you install Plant Applications Web Client.

To open ports on the Plant Applications Core Server, refer to the Port Requirements section in the Getting Started Guide.

Port Description
15672 The default port for the RabbitMQ Message bridge required to communicate with the Plant Applications server for retrieving data updates.
8090/8091 The default port for the Tomcat server.
1433 The default port for the Microsoft SQL server.
9093 The default port for Kafka.
2185 The default port for ZooKeeper.
6984 The default https port for CouchDB.
443/5059 The default port for Web Applications

What to do next: Complete the pre-installation configuration, and then proceed to install the Plant Applications Standard Edition Web Client. See About Installing Standard Web Client.