About Installing Standard Web Client

Installing Plant Applications Standard Edition Web Client installs both the process and discrete applications. You must perform this type of installation if you want to upgrade from a previous version of Plant Applications. You can choose this method for a first-time installation as well.

With the release of Plant Applications 2022 and later, you can now perform a silent installation of Plant Applications Standard Edition Web Client for Windows.

The following table outlines the steps that you must complete to install Plant Applications Standard Edition Web Client for the first time. These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed. All steps are required unless otherwise noted.

Step Task Notes
1 Install Workflow 2.6 SP1 This step is required.
2 Install Plant Applications Server This step is required.
3 Install Operations Hub 2.1 with SIM3 and later
Important:
If using Operations Hub 2022, be aware that after you install Operations Hub you must restart your computer before installing the Plant Applications Web Client.
This step is required.
4 Install and Configure Apache CouchDB This step is required.
5 Ensure that your system meets the requirements for the Standard Web Client installation. This step is required.
6 This step is required.
7 After the Standard Web Client installation, ensure to run the Message Bridge Configuration utility. This step is required.
8 Verify the Installation This step is required.