Set Up Languages for Plant Applications Displays

After installing Plant Applications, you can implement support for additional languages using its Native Language Support (NLS) features.

Procedure

  1. Select All Programs from the Windows Start menu.
  2. In the Proficy folder, select Configure Plant Applications Language Support. Alternatively, you can also run ConfigurePALanguages.exe located at <installation_directory>\Proficy\Proficy Workflow\Program to set up language support.
  3. At the Configure Plant Applications Database screen, modify any server settings as needed.
  4. Select one or more languages to include, then click Save.
    Tip:
    Use these options to set up language support after any subsequent Service pack or SIM upgrade.