The Grid's Weakest Link - or Greatest Opportunity? Why the Distribution Edge is the Frontline of Gri

October 9, 2025

As the world races towards a more electrified future, one part of the grid is being stretched to its limits – and it’s not where most people are looking.

It’s the distribution grid — a burgeoning, complex network of substations, feeders, lateral lines, transformers, and customer interconnection points. This “distribution edge” delivers electricity to homes, businesses, and critical infrastructure, yet remains one of the least modernized and most operationally strained segments of the energy system.

Mounting Pressure on the Distribution Grid
While transmission and generation investments often dominate headlines, the distribution grid quietly carries the bulk of real-world impact. It’s where customers feel outages, where most distributed energy sources (DERs) and renewables connect, and where costs quickly add up. For example, the U.S. Department of Energy’s Quadrennial Energy Review estimates that over 90% of both the frequency and duration of U.S. power outages originate from distribution-system failures — a fact echoed by the National Renewable Energy Laboratory's assessment of grid-edge vulnerability. 

The grid’s limits are being tested by a set of converging factors, including: 

§  Edge Load is Surging: EVs, heat pumps, and industrial electrification are increasing peak demand and temporal load variability across feeders and substations.

§  DER-Driven Disruptions: The rapid growth of DERs on medium-voltage (MV) and low-voltage (LV) feeders is introducing reverse power flows and voltage variability—conditions that stress conventional regulation equipment like on-load tap chargers (OLTCs) and capacitor banks, which were never designed for such dynamic behavior.

§  Aging Assets: Much of today’s distribution infrastructure is over four decades old, built for predictable, one-way flows. Legacy assets and outdated communications are increasingly misaligned with the demands of a fast, data-driven, and decentralized grid.

§  Operational Blind Spots: Many distribution system operators still lack good observability, especially at LV levels, and automation beyond the substation is limited.


As the rest of the grid modernizes, distribution is falling behind—less visible, less resilient. Closing this gap is the next frontier.

End-to-End Grid Coordination
One of the biggest barriers to unlocking the full value of distribution automation lies in how the grid is managed. Historically, Transmission System Operators (TSOs) and Distribution System Operators (DSOs) have worked in silos. But with growing DER penetration and bidirectional power flows, the actions taken at the distribution level increasingly affect transmission-level reliability and market dynamics.

New coordination models are emerging. In Europe, for example, efforts like the ENTSO-E System Needs Analysis and the UK’s Open Networks Project are creating frameworks for near real-time coordination between TSOs and DSOs. In the United States, system operators are actively integrating DERs into wholesale markets through new participation models.

Still, most system operators lack the platforms, protocols, and near real-time data-sharing capabilities needed to seamlessly coordinate across grid layers – a gap that needs to be addressed to fully realize the benefits of automation and decentralization.

From Legacy Systems to Intelligent Grids
Distribution automation uses digital sensors, advanced controls, and fast communication to improve how power is managed and restored at the local level. However, today’s automation is constrained by fixed protection settings, legacy communications, lack of interoperable devices, and centralized control architectures that are not equipped for autonomous, near-instant decision-making.

Edge intelligence, adaptive protection, predictive analytics using ML/AI tools, and integrated, interoperable platforms are key enablers. These capabilities don’t just improve how we monitor and control the grid—they fundamentally reshape how we deliver reliable, affordable, and more sustainable energy in a dynamic operating environment. Solutions like our GridBeats™ Zonal Autonomous Control (ZAC) are part of this next wave—bringing autonomous, edge-based control that complements centralized systems, enabling faster recovery, better power quality, and more localized resilience.

Here’s how automation directly supports the three pillars of the energy trilemma:

  1. Reliability: While technologies like Fault Location, Isolation, and Service Restoration (FLISR) have brought early intelligence to the edge, the next leap in reliability demands faster, adaptive automation—where self-healing zones respond in near real-time and voltage quality is actively maintained amid dynamic power flows. To get there, system operators need more than just high-speed communications; they require edge-native automation platforms, distributed control logic, and interoperable systems capable of making localized, data-driven decisions — restoring power in seconds, not minutes.
  2. Affordability: Automation reduces operational costs by minimizing manual fieldwork (e.g., switching, fault isolation) and defers capital investments through non-wires alternatives (NWAs) like targeted DER dispatch and load flexibility. It also extends the life of critical grid assets—such as OLTCs and capacitor banks—by preventing unnecessary wear from uncontrolled voltage fluctuations.
  3. Sustainability: Building a low-carbon grid requires integrating diverse flexible assets—like renewables, storage, EVs, and smart loads—while maintaining reliability. Advanced automation turns that variability into an asset—enabling near real-time visibility, smarter DER dispatch (e.g., EV load shifting, dynamic inverter control, or feeder-aware battery discharging), and grid services like voltage and frequency support.

 

The Grid’s Next Chapter Starts Here
Solving the energy trilemma won’t happen from the top down, but rather, it will be reengineered from the edge in. With GE Vernova’s GridBeats™ portfolio of cutting-edge automation solutions, we’re embedding intelligence across every layer of the grid—making it faster, more dynamic and future-ready. The energy transition depends on how quickly we reimagine the edge—not as a boundary, but as the new center of innovation.

About the Author

Akanksha Bhat

Akanksha Bhat is a Senior Global Product Manager at GE Vernova’s Grid Automation business, where she leads the strategy for Advanced Automation Solutions that support grid modernization and the energy transition. Her work supports utilities and critical industries in integrating DERs, improving grid reliability, and deploying next-generation automation solutions that enable faster, smarter, and more resilient grid operations. Earlier in her career, Akanksha contributed to national clean energy initiatives at the U.S. Department of Energy’s National Renewable Energy Laboratory (NREL), where she co-authored research on DER integration policy and IEEE 1547-based interconnection rule updates. During her time at Clean Power Research, she led the development of industry-first solutions that assess the impact of extreme weather events—such as wildfires and snowstorms—on solar PV production, enabling smarter investment and risk decisions across the solar value chain. Her academic research includes systems modeling and techno-economic analysis of net-zero energy homes. Akanksha has authored and presented on topics including extreme weather risk assessment, DER Integration, microgrids, and distribution automation. She holds an M.S. in Systems Engineering & Energy Policy from the University of Maryland, College Park, and a B.S. in Electrical and Electronics Engineering from India.

Akanksha Bhat