Power-to-Rack: Why AI Factory Architectures Need a Digital Twin Foundation

March 16, 2026

The rise of AI factories marks a fundamental shift in how we design and operate critical infrastructure. These are not traditional data centers scaled up. They are giga‑scale systems where compute, power, and control operate in tight coordination—and where performance is determined not by individual components, but by how the system behaves as a whole.

This shift changes the role of infrastructure architecture. To deliver speed to deployment, predictable performance, and resilience from day one, AI factory designs must account for dynamic behavior across the entire power system—from energy source to AI rack.

This is not simply a question of capacity. It is a question of architectural confidence.

Reference Architectures as the Foundation for Scale
Reference architectures play an essential role in accelerating AI factory development. They establish proven patterns, define clear interfaces, and provide a common starting point for deploying complex infrastructure at scale. In a rapidly evolving industry, they help align developers, operators, utilities, and technology providers around shared design intent.

AI factories, however, are being deployed across diverse global grid environments—each with unique characteristics, operating practices, and regulatory requirements. Grid strength, inertia, connection timelines, and stability expectations vary widely by region. At the same time, power systems themselves are evolving, with greater reliance on inverter‑based resources, new grid codes, and tighter performance requirements for large, dynamic loads.

In this context, reference architectures are best understood as living frameworks. They define structure and intent while allowing flexibility to adapt to local grid conditions and operational realities. This adaptability is not a weakness; it is a necessary response to complexity.

Reference architectures provide the first, critical step. Their effectiveness increases when they are paired with tools that help translate design intent into real‑world system behavior.

Complementing Design with Real‑World System Insight
While reference architectures establish the “what,” but understanding the “how” requires insight into dynamic system behavior. AI workloads introduce highly synchronized, rapidly changing load profiles that interact with grid infrastructure, on‑site generation, energy storage, and power electronics in complex ways.

By complementing reference designs with system‑level digital representations, designers and operators can evaluate how an architecture behaves under real operating conditions—accounting for regional grid characteristics, transient events, and evolving workload patterns. This approach does not replace reference architectures; it strengthens them by bringing designs closer to the realities they will encounter once deployed.

From Power‑to‑Rack: Designing the System as One
At GE Vernova, we think in terms of “power‑to‑rack”—a holistic view that treats the AI factory as a single, integrated system. This perspective connects energy sources, grid infrastructure, generation, storage, electrification, and the AI rack through a continuous digital thread.

In this model, power is not simply delivered; it is orchestrated. Performance at the rack depends on decisions made upstream—in generation strategies, control logic, and grid interaction. As compute technologies advance rapidly, this end‑to‑end view becomes essential to ensuring that power infrastructure can scale at the same pace as the systems it supports.

To support this power‑to‑rack approach, GE Vernova is developing high‑fidelity, three‑dimensional digital twins of critical grid assets aligned with the NVIDIA Omniverse DSX Blueprint. In collaboration with NVIDIA, this work enables faster, more accurate planning of grid and substation equipment by connecting physical power‑system models directly with the environments in which AI infrastructure is designed, deployed, and scaled. The result is a shared system context where power and compute can be engineered together—early in the design process and with greater confidence.

Validating Architecture Through Virtual Experience
In practice, this shift is already underway. Within GE Vernova, teams are developing high‑fidelity digital representations of power infrastructure that model how AI factories interact with the grid as complete systems—not as isolated assets. These models capture the physics, controls, and operational dynamics that emerge when large‑scale AI workloads meet modern power systems.

By creating virtual environments that reflect real operating conditions, engineers can introduce disturbances, replicate synchronized load spikes, and evaluate alternative architectural choices long before hardware is deployed. Grid events can be simulated, protection schemes exercised, and control strategies refined—without risking uptime or capital.

The impact is critical. Instead of learning exclusively through on‑site operation, teams can design with foresight. This shifts infrastructure development from reactive adjustment to proactive, predictive improvement—and helps ensure that architectural intent translates into real‑world behavior from day one.

Speed to Deployment in a Constrained Grid Environment
Much of the conversation around AI infrastructure speed focuses on supply chains and construction timelines. These remain important, but grid availability and integration are increasingly defining the pace of deployment.

Phased interconnections, interim generation, and evolving grid requirements are becoming standard. The ability to simulate these scenarios in advance allows operators to plan transitions with confidence—improving early‑stage configurations while maintaining a clear path to long‑term operation.

In this way, digital modeling becomes an enabler of speed, not a bottleneck.

Designing for Performance, Resilience, and Confidence
As AI factories scale toward the gigawatt level, the margin for uncertainty narrows. Day‑one performance matters. Stability under dynamic load matters. The ability to adapt to regional grid conditions matters.

Reference architectures provide the foundation. Digital twins complement them by grounding those designs in physics, controls, and real‑world behavior. Together, they enable AI factories to move from concept to operation with confidence—delivering reliable, high‑performance infrastructure that can evolve alongside the AI technologies it supports.

In a world where AI progress is measured in months, the infrastructure behind it must be ready on day one—and resilient for decades to come.

For a deeper system‑level view of how digital twins and AI factory reference architectures work together to accelerate deployment and enable day‑one performance, explore our AI factory power architecture whitepaper here.

About the Author

Vera Silva

Vera Silva is the Chief Strategy and Technology Officer of GE Vernova’s Electrification Systems, a multi-billion global business segment that includes Electrification, Electrification and Storage Systems. In this role, she leads the innovation, technology and business strategy and commercial development. Prior to her role at GE Vernova, Vera Silva was R&D director and senior engineer at Electricité de France (EDF). Preceding EDF she was a research associate in Imperial College London and assistant professor at the Polytechnic Institute of Porto, Portugal. Vera is a highly respected energy industry leader; she has published three books and over 40 scientific papers and was recognized as “Engineer of the Year” in 2016 by the IEEE Power and Energy Society. She is a member of the National Academy of Technologies of France (NATF) and of the U.S. National Academy of Engineering (NAE). Vera holds a Ph.D. in Electrical and Electronics Engineering from Imperial College London and an MSc and BSc in Electrical Engineering & Computer Science from the University of Porto, Portugal.

Vera Silva