Reliability by Design: Why Power Stability is the New Business Case

August 28, 2026

Reliability by Design: Why Power Stability is the New Business Case

A large AI data center can have plenty of installed capacity and still be electrically fragile.

That is the part too many board-level discussions miss. The constraint is no longer just megawatts secured, generators installed, or redundancy tiers specified. It is whether the electrical system can maintain stability while GPU-heavy loads move in ways that disturb the infrastructure feeding them.

For years, most operators treated power as a support function: necessary, expensive, mostly invisible when it works. That model held up when data center loads were comparatively smooth and the main design question was redundancy. The challenge starts when the load itself becomes a source of instability.

The financial impact of data center downtime is no longer just a line item; it is a critical business risk that is accelerating year over year. Power-related failures remain the leading driver of these events1, but the deeper issue is not just the loss of supply. It is that legacy electrical architectures are increasingly inadequate for handling the dynamic, high-volatility demand profiles they were never designed to absorb.

AI Does Not Just Increase Load – it Changes Load Behavior

The growth trajectory of AI alone should force a more serious conversation. The International Energy Agency (IEA) reported that electricity consumption from AI-focused data centers surged 50% in 2025, outpacing broader data center demand growth2. That statistic does not, by itself, quantify short-interval load volatility. But it does reinforce the central issue: AI is changing the electrical profile of the facility, not just increasing aggregate demand.

That distinction matters because the system design needs to change with it. This is no longer a static capacity question, but a question of ramp rate, disturbance isolation, and upstream asset stress.

That has practical consequences.

Gas turbines do not respond well to repeated violent load movement. Utility interconnections are not indifferent to large, fast swings imposed behind the meter. Conventional power conversion and switchgear lineups may be fully adequate on nameplate capacity and still underperform when the duty cycle becomes more erratic than the original basis of design assumed.

This is why the old language around resilience is too soft. The issue is not merely surviving a disturbance. The issue is preventing the facility from creating one.

The Useful Design Move is Decoupling

If the load is volatile, the engineering objective is straightforward: stop that volatility from propagating upstream.

That is where a medium-voltage, series double conversion uninterruptible power supply (UPS) architecture starts to matter. A back-to-back modular multilevel converter system can decouple grid-side dynamics from load-side dynamics3. That is the right frame – not backup power. Decoupling.

Done properly, that architecture creates a controlled electrical boundary. The compute load does not impose every sharp swing directly onto the utility connection or onsite generation, and the sensitive IT process does not have to absorb every grid-side event either. Integrated battery storage then handles short-duration power absorption or injection to smooth transient behavior at that interface3.

That is a more serious answer to AI load volatility than simply adding more downstream redundancy.

This transition redefines the business case for power infrastructure. Rather than functioning as a passive layer of insurance, the system becomes a strategic asset capable of buffering short-term fluctuations. This capability protects upstream assets from unnecessary stress and provides a competitive advantage in navigating utility-led discussions on interconnection, grid curtailment, and compliance with dynamic performance expectations.

This is Where the Financial Argument Gets Real

Power stability should not be framed as a defensive line item.

Smoothing rapid load swings generates measurable commercial value by alleviating stress on upstream equipment, enhancing power management flexibility, and ensuring tighter control through grid-side disturbances3. These factors effectively lower required capacity margins, increase expansion confidence, and strengthen a project’s business case during the critical stages of utility review and final investment approval. In other words, stability is not just a resilience issue.

Stability is part of production economics.

This becomes even more important in projects where power availability already constrains schedule. When major electrical equipment is on long lead times and utility interconnection queues are tightening, any design move that reduces electrical volatility has value beyond uptime. It protects schedule certainty. It protects the expansion thesis. It protects the assumptions behind the revenue model.

Steel Matters Here for a Reason

The most credible proof-point for this architecture does not come from a data center, it comes from steel. Electric arc furnace operations are one of the clearest examples of an electrical environment where extreme dynamic behavior is exposed immediately. These loads are abrupt, punishing, and intolerant of weak control architecture. If a power electronics platform has proven itself there, that matters.

Steel mills and AI data centers are not identical, but they share a core challenge: both create highly dynamic loads that place unusual stress on the electrical system feeding them. While other solutions are still being tested in this new environment, this architecture was forged in one of the harshest electrical settings in industry. It was shaped by a hostile reality rather than a marketing brief. That pedigree provides a level of proven stability that no lab-tested pilot can match.

Don’t Wait for the Outage to Clarify the Risk

The old model treated power as a cost center with redundancy attached. AI is exposing the flaw in that thinking.

If the electrical system cannot absorb fast load movement without destabilizing the assets around it, then power is no longer a background utility, but part of the core production system.

Design it that way.

This is where the strategic argument gives way to engineering reality. In the next piece, we’ll compare the electrical demands of steel and AI data centers directly and show why a platform built for one of the harshest load environments in industry matters here.

References

  1. Uptime Institute, Annual Outage Analysis 2026, May 2026
  2. International Energy Agency (IEA), Key Questions on Energy and AI – Executive Summary, 2026, https://www.iea.org/reports/key-questions-on-energy-and-ai/executive-summary
  3. GE Vernova, Fact Sheet: MV-UPS Power Stability, August 2026. 

About the Author

Ed Torres

Edgardo Torres, a distinguished leader at GE Vernova, spearheads the Power Conversion & Storage business. With a career spanning over three decades, Ed has been a forward-thinking leader, guiding the business toward innovative power conversion and energy storage solutions that are essential for modern energy systems. More recently, Ed has drawn on Power Conversion & Storage's deep expertise in complex, bespoke electrical systems and advanced energy storage integration to successfully pivot the business strategy toward power stability and flexibility – a critical and growing requirement for both utility and industrial customers as they navigate power reliability in an increasingly renewable energy landscape. Ed’s GE Vernova journey began in 1997 on the company’s TLP Edison program, placed with GE’s Consumer & Industrial business in Louisville, Kentucky. While there he worked in several engineering roles, mainly focused on NPI, redesigning products for manufacturing in Mexico and factory relocations. In 2001, Ed joined GE Gas Power, where he held various roles in quality, risk management, and commercial operations across diverse locations, including Italy, Mexico, and the United States. In 2010, he was appointed General Manager, Latin America for Measurement & Control (now Nexus Controls) and relocated to Brazil, where he later became President & CEO of GE Oil & Gas Turbo Machinery Solutions Latin America (now part of Baker Hughes). Additionally, Ed is the Executive Sponsor for the LAAN Latin American Allies Network in France and Europe. Born in San Juan, Puerto Rico, Ed attended Carnegie Mellon University, Pittsburgh and graduated with a B.S. degree in mechanical engineering in 1997. In 2006, he earned his executive MBA from Emory University, Atlanta.

Ed (Edgardo) Torres