Unlocking Resilient Grids Through AI/ML-Driven Virtualization

October 1, 2025

The power grid has entered a transformative era. Traditional infrastructure – once built around predictable, one-directional electricity flow – is being reshaped by new realities that include distributed energy resources (DERs), electrification, digitalization, and more frequent extreme weather events. These changes demand not just incremental improvements, but a rethinking of how grids are protected, automated, and operated.

At the heart of this transformation lies virtualization: the ability to move critical protection and control functions from physical devices into flexible, software-defined systems. Combined with the power of artificial intelligence and machine learning (AI/ML), virtualization is redefining how utilities can deliver power reliability, scalability, and resilience while facing unprecedented change.

Why Virtualization Matters
Historically, grid operations have relied on hardware-dependent solutions. While robust, these systems also come with limitations: longer upgrade cycles, high replacement costs, and difficulty scaling as grid complexity grows.

Virtualization changes this. By decoupling functions from physical hardware, utilities can centralize and distribute intelligence as needed. This means faster operation and maintenance, mitigation of failure, and an ability to have protection and automation blend seamlessly across the entire electrical network. Ultimately, virtualization unlocks:

Flexibility: Software-defined tools that can be deployed, updated, or (re)configured without major hardware overhauls.
Resilience: The ability to shift functions, ensuring continuity even when parts of the system are compromised.
Scalability: Support for the growing demand and number of DERs as well as dynamic loads like electrical vehicle charging.

This marks a fundamental shift in how grids are designed to anticipate, absorb, and adapt to change.

From Reactive Recovery to Proactive Protection
In the past, grid resilience was often measured by how quickly operators could react after an outage. Today, with AI and virtualization, the focus has shifted to proactive protection.

Imagine a severe storm approaching a coastal zone. Instead of waiting for equipment to fail, AI-powered models can forecast impact, trigger backup systems, and reroute power – all before the first transformer goes down. The result? Based on the results of a customer collaboration project, recovery times reduced by up to 70%, costs were contained, and customer impact was minimized.

This proactive approach isn’t science fiction – it’s the future. A future that’s already here and being shaped by AI/ML. These technologies are already proving their value in analyzing massive data sets, predicting system behavior, and enabling automated decision-making that human operators cannot alone achieve.

Technology Trends
There are several technology trends that are accelerating the shift we are seeing:
- AI/ML: More sophisticated algorithms that can predict failures and enable adaptive responses.
- Cloud and edge computing: The flexibility to run virtualized functions either centrally in the cloud or more locally at the edge, depending on the need.
- Advanced communications: High-speed, secure data exchange.
- Cybersecurity: Enhanced cybersecurity measures embedded into the system to protect against digital threats as well as physical disruptions.

Together, these advances are creating a new foundation for grid operations – one that is not only capable of managing today’s challenges, but also adaptable to tomorrow’s uncertainties.

Business Impact: From Centralized to Distributed Intelligence
As DERs become increasingly mainstream, the grid’s architecture is evolving. A distributed model is emerging, where multiple nodes work in coordination - communicating and adjusting in near real-time. This approach enhances resilience, reflecting the decentralized nature of modern energy systems. In this context, a centralized architecture — where a single node manages control across the entire grid — is no longer viable everywhere. While centralized control provides strong oversight, it also introduces risks of bottlenecks and single points of failure.

GE Vernova’s GridBeats™ portfolio of software-defined solutions showcase how these architectures can operate in tandem. By coordinating controllable loads and DERs, GridBeats™ enables autonomous distribution, allowing the grid to dynamically balance supply and demand, reduce stress during peak periods, and ensure that energy is delivered where it’s needed.

For utilities, the business case is evident: virtualization and distributed intelligence lower operational risk, accelerate the integration of renewables, and open new pathways for grid modernization.

Looking Ahead
Transitioning to an intelligent grid will be a journey, not a destination. Utilities will adopt new technologies at various paces, guided by local regulations, existing infrastructure, and customer needs. While some might begin with centralized architecture, some may leap directly into distributed models.

The one common goal? A grid that is more flexible, more sustainable, and more resilient. At GE Vernova, we see virtualization as a cornerstone of this journey. By integrating advanced intelligence into grid operations, operators can go beyond traditional limits into embedded capability.

Virtualization and AI are no longer theoretical concepts – they are practical tools already shaping how utilities operate across the globe. Adopting these technologies goes beyond modernization, but also future-proofs the grid against an era defined by change. While the challenges are significant, so are the opportunities, and by embracing virtualization and AI, we can unlock new levels of agility, resilience, and customer value.

Stay tuned for my upcoming whitepaper, where I’ll take a deeper dive into the technologies, architectures, and real-world case studies driving this transformation. 

About the Author

Claudia Cosoreanu

Claudia is the Chief Technology Officer, Grid Automation at GE Vernova, where she leads the vision and strategy for AI/ML empowered grid technologies. In this role, she is focused on advancing innovation across digital substations, grid intelligence, automation services, and cybersecurity— enabling utilities & industries to modernize their infrastructure, increase grid resilience, and accelerate the energy transition. She works closely with global teams and customers to shape technology roadmaps that enable higher renewable penetration, reduced maintenance costs, and improved operational uptime. Claudia holds a Master of Science in Mechanical Engineering with a focus on Automation & Control, as well as an MBA in Marketing. She has been recognized with the 2009 Women in Technology and the 2015 Corporate Technology Staff Leadership Awards within GE Vernova. Claudia is also the holder of three patents in the energy industry.

Claudia Cosoreanu