Valley city at night under moonlight, symbolizing reliable energy through GE Vernova grid solutions

Press Releases

GE Vernova wins multiple orders of high-voltage power transformers and reactors from India’s largest transmission utility

July 20, 2021
  • GE Vernova wins multiple orders of 765 kV transformers and reactors from Power Grid Corporation of India Limited (PGCIL)
  • GE Vernova will produce 45 units of 765 kV transformers and reactors for the new substations to be set up in the Indian state of Rajasthan by PGCIL, for evacuating 8.1 gigawatt (GW) of green power from the state’s solar energy zones
  • The project’s transformers and reactors will be supplied by GE Vernova's Grid Solutions’ state-of-the-art power transformer manufacturing facility in Vadodara, India

New Delhi, India and Paris, France, July 20, 2021:  GE Vernova Renewable Energy’s Grid Solutions business (NYSE: GEV) announced today it has recently been awarded multiple orders to supply 765 kV transformers and  reactors in India. The contracts have been awarded by  Power Grid Corporation of India Limited (PGCIL), India’s largest state-owned transmission company. As part of the order, GE Vernova will provide 13 units of 765 kV transformers and 32 numbers of 765 kV reactors.

GE Vernova’s transformers and reactors will be installed in the new substations that will be set up in the Indian state of Rajasthan by PGCIL, to evacuate 8.1 gigawatts (GW) of power from the state’s solar energy zones under Phase-II of the Transmission System for evacuation of power from solar energy zones in Rajasthan project. This includes the evacuation of energy from four solar energy zones within Rajasthan for onward dispersal of power to various beneficiaries - 1.05 gigawatts (GW)  from Bhadla, 2.2 gigawatts (GW)  from Fatehgarh, 1.9 gigawatts (GW)  from Ramgarh and 2.95 gigawatts (GW) from Bikaner.

Rajasthan, located in northern India, receives maximum solar radiation intensity with very low average rainfall. It also has an abundance of desert and uncultivated lands, making it the ideal place for solar energy generation. Due to these geographical and environmental advantages, Rajasthan is emerging as a leader in renewable energy generation among the Indian states.  India’s government has set a target for establishing 175 gigawatts (GW) renewable capacity by 2022, which includes 100 gigawatts (GW)  from solar and 60 gigawatts (GW)  from wind. This includes the solar generation potential of about 20 gigawatts (GW) in Rajasthan.

Pitamber Shivnani, President & CEO, GE Vernova’s Grid Solutions, South Asia, said: “With a persistent focus on decarbonization and round-the-clock power, we believe that the Indian energy landscape will continue to undergo a significant positive transformation. The transmission system for evacuation of power from solar energy zones in Rajasthan is an excellent initiative by India’s government to promote the use of green energy. As a leader in grid modernization solutions, we are always proud to join hands with valued customer Power Grid Corporation of India to implement innovative solutions that will help India accelerate its energy transition journey.”

Reinforcing GE Vernova’s commitment to the Government of India’s ‘Make in India’ vision, this project’s transformers and reactors will be supplied from GE Vernova's Grid Solutions’ state-of-the-art power transformer manufacturing facility in Vadodara, India. GE Vernova’s comprehensive suite of power transformers support a wide range of voltage levels with applications in generation and transmission. GE Vernova’s power transformer technology provides several benefits to customers, including exceptional performance, quality and reliability with digitized protection and monitoring schemes and advanced design and testing capabilities.