GE Vernova delivers materials and eco-design studies for high voltage solutions to accelerate insulation and environmental innovation. GE Vernova’s services provide the expertise and methods that enable new value to support customer engineering, sourcing, quality control and EHS activities.

The technical studies, tests and impact evaluations support:

  • development of many types of insulation material for HV applications
  • analysis of corrosion and metallic material
  • reduction of environmental footprint

GE Vernova’s studies are compliant with customers and international standard.

Materials and Eco-Design Studies

For High Voltage Solutions

GE Vernova delivers materials and eco-design studies for high voltage solutions to accelerate insulation and environmental innovation. GE Vernova’s services provide the expertise and methods that enable new value to support customer engineering, sourcing, quality control and EHS activities.

The technical studies, tests and impact evaluations support:

  • development of many types of insulation material for HV applications
  • analysis of corrosion and metallic material
  • reduction of environmental footprint

GE Vernova’s studies are compliant with customers and international standard.

Reducing Environmental Footprint

Eco-Design

  • Life cycle assessment
  • Environmental regulations studies
  • End-of-life manuals
  • Eco-design methodology training

Inspections & Homologations

  • Characterization of solid, liquid and gaseous materials
  • Compatibility tests
  • Supplier homologation
  • Material homologation
  • Post event analysis
Analyzing Corrosion & Metallic Materials

Investigation

  • In-depth investigation of corroded parts and corrosive material
  • Moist heat cycling, salt fog tests
  • Mechanical tests, microscopy

Anti Corrosion

  • Selection of the anti corrosion coating including paint and grease

Material Selection

  • Selecting the correct material class based on atmosphere corrosivity
Supporting Development of Insulation Materials

Solid Insulation

  • Mechanical characterizations
  • Thermal and electrical aging studies
  • Lifetime study

Liquid Insulation

  • Development of mineral and ester oils
  • Diagnostic techniques
  • Composite systems

Gaseous Insulation

  • Development of environmentally friendly gas and mixture
  • Gas analysis: new and arced SF6 and g3

The R&D studies support the development of many types of insulation material, provide corrosion and metallic material analysis and help reduce the environmental footprint of equipment and technologies. Type of materials supported:

Solid Insulation

  • Epoxy
  • Thermoplastics
  • Composite insulators
  • Ceramic insulators

Liquid Insulation

  • Mineral oil
  • Ester oil
  • Silicone oil

Gaseous Insulation

  • SF6
  • Environmentally friendly alternative

Benefit of Working With The “Disruptive” Team With Extensive Expertise

Studies are delivered by GE Vernova’s Subject Matter Experts based in the Global Technology Center. The team is active in international working groups and delivers lectures at technical conferences including CIGRÉ, Matpost, IEEE, CEIDP, IEC.

The GE Vernova materials and eco-design team members have filed over 35 patents in the last 15 years and bring disruptive technologies to the industry, examples include: