The WEATHER TREND section contains a trend chart of the site irradiance, ambient temperature, and the average module temperature.
Procedure
- Access the Solar Accelerators home page.
The OVERVIEW section appears.
- In the WEATHER section, select
.The
WEATHER TREND section appears, displaying a trend chart of the site irradiance (POA irradiance), average module temperature, and the ambient temperature. If you pause over the chart, the aforementioned values at that point appear.

- By default, the data is displayed for the past one week. To filter the data based on a date range:
- Use the quick filter options (such as 1 DAY, 3 DAYS, 1 WEEK, and 4 WEEKS) to filter the data quickly.
- Click and drag the portion below the chart to zoom in or zoom out the duration.
- To download the data into a PNG or a CSV file, select
, and then select the required format.