Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / CCriteriaStringModifier Class / CriteriaFromString Method


CriteriaFromString Method (CCriteriaStringModifier)
Retrieves the sampling mode, calculation mode and query modifiers from criteriaString
Syntax
Public Function CriteriaFromString( _
   ByVal criteriaString As System.String, _
   ByRef criteria As DataCriteria _
) As System.Boolean

Parameters

criteriaString
criteria

Return Value

A string representation of this instance.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also