Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ClientMessageContext Class / GetServerVersion Method


GetServerVersion Method
Syntax
Public Shared Function GetServerVersion( _
   ByVal session As System.String _
) As System.Version

Parameters

session
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also