Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQueryParams Class / ToString Method


ToString Method (DataQueryParams)
Converts the value of this instance to a System.String.
Syntax
Public Overrides Function ToString() As System.String

Return Value

A string representation of this instance.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also