Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / EnumeratedSet Class / EnumeratedState Property


EnumeratedState Property
List of all States in the set.
Syntax
Public Property EnumeratedState As System.Collections.Generic.List(Of EnumeratedSetState)
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also