Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ICollectors Interface / Browse Method
A collector name.
Browse position.
Wildcard expression matching tag descriptions.
Wildcard expression matching source addresses.
Whether to recurse.


Browse Method
Initiate a tag browse in a collector via a Historian server.
Syntax
Sub Browse( _
   ByVal collectorname As System.String, _
   ByVal position As System.String, _
   ByVal descriptionmask As System.String, _
   ByVal addressmask As System.String, _
   ByVal recursive As System.Boolean _
) 

Parameters

collectorname
A collector name.
position
Browse position.
descriptionmask
Wildcard expression matching tag descriptions.
addressmask
Wildcard expression matching source addresses.
recursive
Whether to recurse.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also