Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataStores Interface / Set Method
Name of the data store
Whether this data store is the default store (to be used as default data store for tags adds, and archive related operations)
Description of the data store
Type of the data store


Set Method (IDataStores)
Apply properties from the given dataStore to a Historian server.
Syntax
Sub Set( _
   ByVal dataStoreName As System.String, _
   ByVal isDefault As System.Boolean, _
   ByVal description As System.String, _
   ByVal storageType As DataStore.DataStorageType _
) 

Parameters

dataStoreName
Name of the data store
isDefault
Whether this data store is the default store (to be used as default data store for tags adds, and archive related operations)
description
Description of the data store
storageType
Type of the data store
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also