Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IMessages Interface / Add Method
New message to add.


Add Method (IMessages)
Adds a new audit message to a Historian server.
Syntax
Sub Add( _
   ByVal message As Message _
) 

Parameters

message
New message to add.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also