Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / MultiFieldValue Class / NumFields Property


NumFields Property
NumFields in the MultiFiled Type.
Syntax
Public Property NumFields As System.Integer
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also