Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / PagedQuery Class / Continuation Property


Continuation Property
Whether additional results are available in the server for this query.
Syntax
Public ReadOnly Property Continuation As System.Boolean
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also