Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / VersionHeaderBehavior Class / VersionHeaderBehavior Constructor / VersionHeaderBehavior Constructor(ServerConnection)


VersionHeaderBehavior Constructor(ServerConnection)
Syntax
Public Function New( _
   ByVal clientServerConnection As ServerConnection _
)

Parameters

clientServerConnection
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also