Optimize Performance
About this task
- Optimize virtual memory: Through the use of paging files, Windows
allocates space on your hard drive for use as if it were actually memory. This
space is known as virtual memory. This topic describes how to optimize the
virtual memory on the Historian archiver computer. Note:If the paging file is set to grow dynamically, your system may experience severe performance problems during runtime. To ensure optimal performance, the Initial Size and Maximum Size values for the paging file must be the same so that the paging file does not grow dynamically. For more information on creation and sizing of Windows paging files, refer to Microsoft Windows Help.
- Optimize the server performance: If the file sharing and printer sharing options on the computer on which you want to install Historian is set to maximize data throughput, it can lead to excessive paging when dealing with large files, which can interfere with applications like Historian. You can change these settings to optimize the performance.
Procedure
-
To optimize virtual memory:
- Access Control Panel, and then select .
- Under Performance, select .
- Under Virtual Memory, select Change.
- In the Initial size and Maximum size fields, enter a value equal to three times your physical memory.
- Select Set, and then select OK.
-
To optimize server performance: