Line Chart
In a line chart, data points are connected by a line to help visualize the changes in data trends over a period a time.
Operations Hub New Layout | Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub. |
Operations Hub Classic Layout | Refer to About Widgets |
Line Chart Properties
Field Name | Description |
---|---|
Line Type | Select from the available list of chart line types. Each chart type
provides the best visual representation based on the data and context.
|
Source > Data Source | See Set Up Data Binding for Widgets |
Use Raw Format | Select the check box to display numbers in raw format. For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off. |
Number of Decimals | This option appears if you do not want to display numbers in raw
format. In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number. |
Title | Title name for the chart. |
Subtitle | Subtitle name for the chart. |
Y Axis Title | Title name for Y-axis. |
Y Axis Limits | Select the check box for Enable Limits if you want
to define a data range for the Y-axis of a line chart. By setting the minimum (Min) and maximum (Max) values for the Y-axis, you can ensure that the line chart shows data within that range, which can be useful for highlighting specific trends or patterns within the data. Enter values for the following fields:
|
X Axis Title | Title name for X-axis. |
X Axis Mode | Format the X-axis:
|
X Axis Rotation | If you choose to rotate labels, enter the degree of rotation. |
X Axis Data Format | Lets you choose how the data on the X-axis is displayed. Select
String:
Select Date:
|
X Axis Date Format | This option is irrelevant if your data format is
String. You should leave this field empty. If your data format is Date, enter a valid date format to avoid displaying Epoch time. Some examples are:
|
Enable Line Limits | Select/Clear the check box to show/hide line limits. If you choose to show line limits at runtime, then enter the HiHi, Hi, Lo, LoLo limit values. |
Labels External | When checked, the limit labels move outside the chart area. When unchecked, the labels remain inside the chart area. |
HiHi Label | Enter a label name for HiHi limit. |
HiHi | Use the available options to configure the source values. Refer to Set Up Data Binding for Widgets. |
HiHi Color | Select a HiHi line color. |
Hi Label | Enter a label name for Hi limit. |
Hi | Use the available options to configure the source values. Refer to Set Up Data Binding for Widgets. |
Hi Color | Select a Hi line color. |
Lo Label | Enter a label name for Lo limit. |
Lo | Use the available options to configure the source values. Refer to Set Up Data Binding for Widgets. |
Lo Color | Select a Lo line color. |
LoLo Label | Enter a label name for LoLo limit. |
LoLo | Use the available options to configure the source values. Refer to Set Up Data Binding for Widgets. |
LoLo Color | Select a LoLo line color. |
Legend | Select the Visible check box if you want to show
the chart legend. You can also use the vertical/horizontal options to position the legend in the chart. |
Crosshair | Select the check box if you want to show the crosshairs in the chart. |
Show Points | Select the check box if you want to show data points in the chart. |
Point Symbol | Select from the available list of symbols to represent the points in the chart. |
Stacking |
|
Truncate X-Axis | Select the check box to truncate the X-axis labels. |
Palette | Provides a list of built-in themes that help apply consistent color
schemes across widgets, allowing you to quickly customize their look. Each
theme comes with its own set of unique colors, defining the visual appearance
of the widget.
Note: This feature is currently available only for a
select few widgets. |
Hidden | Select this check box if you want to hide the widget.
To show the hidden widget in Operations Hub new
layout, go to Page Visuals
and under Action column,
select ![]() |
Configuring Source Values for Line Charts
When configuring a line chart using an extension query, the data retrieved from the data source is automatically arranged in the following manner: first, the Timestamp, followed by the Value, and then the Name.
- Timestamp: This data is used for the X-axis.
- Value: This data is used for the Y-axis.
- Name: This data is used for legend labels.
- Timestamp/Week for the X-axis
- Value for the Y-axis data
- Name for the legend
Chart Line at Runtime
+
for
timestamp.
-
for
timestamp.