Pie Chart
Operations Hub New Layout | Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub. |
Operations Hub Classic Layout | Refer to About Widgets |
Pie Chart Properties
Field Name | Description | ||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Pie Type | Select from the available list of pie charts. | ||||||||||||
Data Source | Provide the input data source for the chart either manually or through
data binding. Note: If configuring data source manually, ensure that the
first output field is always a 'value' and the second is a
'string'. If binding data through drag-and-drop method, you don't need to do anything. The order of the fields is automatically handled. |
||||||||||||
Title | Title name for the chart. | ||||||||||||
Subtitle | Subtitle name for the chart. | ||||||||||||
Series color configuration - manual | You can use this property to manually define the colors used in a pie
chart. For example, a dashboard visualizing the status of machines on a production line uses a pie chart where each machine's status is identified by a unique tag, and can be Operational, Under Maintenance, or Idle. To set up the pie chart with default colors to represent the
statuses:
|
||||||||||||
Legend | Select the Visible check box if you want to show the chart legend. You can also use the options to position the legend in the chart. | ||||||||||||
Show Labels | Select the check box if you want to show labels in the chart. | ||||||||||||
Show Tooltips | Select the check box if you want to show tool tips in the chart. | ||||||||||||
Show Name | Select the check box if you want to show label name. | ||||||||||||
Show Value | Select the check box if you want to show values in the tooltip. | ||||||||||||
Show Percentage | Select the check box if you want to show percentages in the tooltip. | ||||||||||||
Hidden | Select this check box if you want to hide the widget.
To show the hidden widget in Operations Hub new
layout, go to Page Visuals
and under Action column,
select ![]() |
Note:
When exporting a chart to JPEG or PDF at runtime, make sure your browser's zoom is
set to 100% or above.