Histogram
This plug-in provides a graphical representation of the distribution of numerical data.
Operations Hub New Layout | Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub. |
Operations Hub Classic Layout | Refer to About Widgets |
Histogram Properties
Field Name | Description |
---|---|
Source > Default Sampling Mode | Set a default sampling mode for histogram. See Set Up Data Binding for Widgets |
Source > Height | Set the height of the histogram chart. See Set Up Data Binding for Widgets |
Source > Chart Title | Provide a title name for the histogram chart. The value must be a text string. See Set Up Data Binding for Widgets |
Source > Show Header Controls | Specify a boolean value. True shows chart header
controls. False hides chart header controls. See Set Up Data Binding for Widgets |
Source > Scroll Percentage | Configure the scroll percentage based on the total time range. |
Background Color | Adds a background color to the histogram chart. |
Show Border | Select the check box to add a border to the histogram chart. |
Border Color | If you choose to add a border, then set a color for the border. |
Source > Logging Level | Applies to log messages. You can control the level of data logged to the
browser console. The default value is info . Other valid values
are step , trace , debug ,
warning , error , and
none . |
Source > Historian Legend | Specify whether to show/hide legend by default. |
Number of Bins | Enter the default number of bins to appear on histogram. |
Bins Color | Set a default color for the bins. |
Normalized Curve Color | Set a default color for the normalized curve. |