Enterprise Deployment Architecture

The following diagram shows the recommended deployment architecture for Enterprise Edition Web Client Installation. In this diagram, the various servers suggest the order of installation of the various software packages on their respective servers. We recommend that you follow the same order.

If, however, you choose the minimum-number-of-servers configuration for the deployment, resolve the following possible port conflicts:
  • Operations Hub and Plant Applications Web Reports: Operations Hub uses 443 as the port number for https binding. Therefore, use a different port for the Web Reports server.
Note:
If port 5986 is used by any other application, then modify the default.ini file of Apache CouchDB to set the port number under httpd to 5987.