SQL Server Requirements

Note:
Passwords for recent versions of SQL Server are case sensitive. Ensure passwords are updated if upgrading from a version older than 2008.

SQL Server Installed Components

The following components must be installed with MIXED MODE security:
  • Database Engine Services

SQL Server Naming Conventions

Do not use special characters for server names.

SQL Server User Access

As an SQL Server user, you must have following permissions to install or upgrade the Plant Applications Server successfully.
  1. SYSADMIN Server role.
  2. MINIMUM SQL Server User Accesses required to install or upgrade Plant Applications when SYSADMIN Server role is not available for the Database User.

    To install Plant Applications, the following configurations are required for the database user:

    1. Server Role:
      • processadmin
      • public
      • setupadmin
    2. Mapping for Database User with Server Roles

      For example:

      For This Database Use This Database User Role
      msdb
      • public
      • SQLAgentUserRole
      Plant Applications Database (SOADB)
      • db_owner
      • public
      tempdb public
    3. Securables

      You can set the following permissions (WITH GRANT) for the database users:

      • Connect Any Database
      • Alter any login
      • Connect SQL
      • Create any database
      • View any definition
      • View any database
      • View server state
      Note:
      For msdb users, you must give access to the following with permissions as shown in the table:
      Access To This Permission
      Table Select 'WITH GRANT'
      View Select 'WITH GRANT'
      Stored procedure Execute 'WITH GRANT'

Supported SQL Server Cloud

The following versions (or flavors) of SQL Server Cloud are supported:

  • AWS Relational Database Service (RDS)
  • Azure SQL Managed Instance
  • NOTE: Azure SQL Database is not supported

Supported Network Protocols

Before installing SQL Server, the stand-alone named and default instances must support the following network protocols:

  • Shared memory (Shared memory is not supported on failover clusters)
  • Named pipes
  • TCP/IP

The same network protocol must be set up on the server and client computers to be able to communicate with each other.

SQL Server Browser Service and Plant Applications Server

Microsoft System CLR Types SQL Server 2016 (32-bit only) must be installed.

If you are installing Plant Applications Server on a computer and SQL Server on a different computer, the SQL Server Browser service (sqlbrowser) must be running before installing Plant Applications Server.

For information on the SQL Server Browser service, see: http://msdn2.microsoft.com/en-us/library/ms165724.aspx

Enabling TCP/IP and XP_cmdshell

The xp_cmdshell option and the TCP/IP protocol, which are disabled by default, must be enabled. The installation process verifies whether the TCP/IP protocol is enabled and if it is not enabled, a message box appears asking permission to enable the TCP/IP protocol. If permission is denied, the installation process will quit. The xp_cmdshell option is automatically enabled during the installation process.

Note:
If you are installing Plant Applications Server on a computer and SQL Server on a different computer, you must manually enable the TCP/IP protocol. It cannot be enabled remotely.