Operation Status Indicators
The status of an operation indicates the progress of work for the operation.
In the Unit Operations module, the status of an operation is automatically determined and displayed
with a color-coded indicator. The following table provides a list of status indicators
defined for an operation.
Status | Status Code | Status Indicator | Description |
---|---|---|---|
Ready | 20 | ![]() |
Indicates that the serial/lot is available for you to perform the operation. |
Clocked on by you | 30 | ![]() |
Indicates that the serial/lot is currently clocked on only by you for the operation. |
Clocked on by another user | 30 | ![]() |
Indicates that the serial/lot is currently clocked on by another user for the operation, but is not clocked on by you. |
Clocked on by other users | 30 | ![]() |
Indicates that the serial/lot is currently clocked on by multiple users for the operation, but is not clocked on by you. |
Clocked on by you and other users | 30 | ![]() |
Indicates that the serial/lot is currently clocked on by you and other users for the operation. |
Clocked on by other users in the past | 30 | ![]() |
Indicates that work for the serial/lot has begun, but the serial/lot is currently not clocked on for the operation. |
On hold | 30 + (OnHold flag = true) | ![]() |
Indicates that the operation is in the On Hold status. This status indicator appears when a defect has been created for the serial/lot for the operation. After the defect is closed, the status of the operation is modified to the original status and the operation appears in the Open page. |
Complete | 40 | ![]() |
Indicates that the operation is in the Complete status. This status
indicator appears when an operation, the quality variables associated with
the operation, and the mandatory BOM items associated with the operation are
completed for the serial/lot. Note: Defining quality variables and BOM items
for an operation are optional. However, if they are defined, they must
be completed for all the serials/lots in the operation. |
Skipped | 60 | ![]() |
Indicates that the operation is in the Skipped status. |
Excluded | 70 | ![]() |
Indicates that the operation is excluded from a mutually exclusive operations set. |