About the Unit Operations Application
As an operator, you can use the Unit Operations application in the Plant Applications Web Client to access the operations associated with a work order. Each row in the Unit Operations page represents an operation to be performed or has been completed. By default, the Unit Operations application contains the operations of the Machine that you select.
On the Unit Operations page, in the Machines drop-down list, by default the route enabled units that you have assigned to your profile (in the My Machines application) are displayed. If you want to view the entire list of route enabled units, you must set displayMymachineUnits property value to False in the operator-app-prod.yml properties file of Unit Operations. By default, the displayMymachineUnits property value is set to True, that is, only the route enabled units that are assigned to your profile in the My Machines application are displayed.
- Access an operation.
- Clock on an operation.
- Clock off an operation.
- Add a Comment
- Access a list of BOM parts associated with a serial or lot.
- Specify the consumption of BOM parts during production.
- Create a lot.
- Specify a Quality Variable
- Add a Tool to an Operation
- Provide the Completed Quantity for an Operation
- Mark an Operation Complete
- Skip an Operation
- Create a non-conformance.