View the Details of an Event

You can access the Events Details report of an event by selecting an event in the Waste page. The report provides all the details relevant to the selected event in the following sections:
  • Event Information
  • Waste Cause Information
  • Waste Variables

Event Information

This section displays the generic details about the waste event and consists of the following fields:
FieldDescription
EventThe production event to which the waste is associated. By default, 500 records will be displayed. As you scroll down and reach the end of the list, you can select More to display 500 more records.
Note:
This field is populated only for a production-based event. In case of a time-based event, this field is blank.
Created OnThe date and time the waste event record was created.
Updated OnThe date and time the waste event record was updated.
AmountThe amount of waste that was generated for the event.
UnitsThe unit of measurement that correspond with the amount of generated waste.
ProductThe product that was being produced.
Added ByThe name of the service or person who created the waste event.

Waste Cause Information

This section displays the details of the waste that was generated and consists of the following fields:
FieldDescription
LocationThe specific piece of equipment along a production line that caused the waste.
FaultThe error in the processing stream or equipment that led to generation of waste.
TypeThe physical state of waste that was generated.
Waste ReasonThe reason that describes the cause of the waste.
Waste ActionThe corrective action taken to fix the fault that caused the waste.

Waste Variables

This section splits the production event into different timelines according to the amount of waste that was generated every time the production event was triggered. The final entry displays the overall waste that was generated for the entire production event.