About Submitting Inspection Results
After you perform an inspection, you must review the results to perform the following tasks:
), and it appears in the Closed section. You can no longer modify the inspection.
- If the inspection results of a sample fall under the specified limits, accept the serial/lot.
- If the inspection results of a sample do not fall under the specified limits and/or the material
is defective:
- Create a non-conformance for the material lot. When you do so, a defect is created for each defective serial/lot in the material lot and linked to the non-conformance. The non-conformance and the underlying defects appear in the Non-Conformance application.
- Dispose all the defects in the non-conformance.
Note:You can now select multiple serials/lots and update the status simultaneously.