Access Serial/Lot Details

Procedure

  1. Log in to Plant Applications Web Client.
  2. Select Genealogy.
    The Genealogy page appears allowing you enter a serial/lot number.
  3. In the Enter a Serial/Lot# box, enter a serial/lot number for which you want to view the details.
    Tip:
    To search for an activity using a barcode, select for an option and scan for the barcode specific to the option. Use your device's front camera only for Barcode/QR code scanning. The application supports one-dimensional (Aztec, Data Matrix, MaxiCode, PDF417, UPC-A, UPC-E, UPC/EAN Extension) and two-dimensional (Codabar, Code 39, Code 93, Code 128, EAN-8, EAN-13, ITF, QR Code, RSS 14, RSS Expanded) types of standard codes.
    Note:
    In an iPad, you can use only in the Safari browser.

    Select .

    An entry with the entered serial/lot number in the left side panel appears and associated details appear in the right panel.
    Note:
    If the entered serial/lot number has associated serial/lots or events, you can expand by selecting the arrow icon to view the hierarchy of raw consumption. You can select any specific serial/lot to view its details in the right panel. The following table provides the header details of the selected serial/lot. However, the source details of the serial/lot and where it has been used can be viewed in the Source Details (source details) and Used in tabs respectively.
    Label Description
    Serial/lot# The serial/lot for which you want to access the details.
    Material The material of the serial/lot.
    Material Desc The material description of the serial/lot.
    Status The status of the serial/lot.
    Material Family The material family of the serial/lot.
    Location Specifies the location of the serial/lot.
    Initial Qty The initial number of items in the serial/lot.
    Current Qty The current number of items that are useable and available quantity of the serial/lot after consumption.
    Note:
    The current quantity differs from initial quantity if quantity of the serial/lot is consumed through the manufacturing processing of a different material, some quantity of the lot was scrapped, or so on.
    Select if you want to collapse the side panel.
    Select to refresh the selected serial/lot in the left panel and associated details in the right panel.
  4. By default, the tab (Source Details ) that displays the related Work Order, Process Order, Receiver, or Production Event details is selected.
    Note:
    Source Details is replaced with Work Order, Process Order, Receiver, or Production Event based on the source of that serial/lot’s manufacturing)
  5. Select the Used in tab to view where the serial/lot was used.
    The following details appear displaying all the associated serial/lots that consumed some quantity of the serial/lot selected in the left panel.
    Note:
    You can drill into details about the individual serials/lots that are consumed for the selected serial/lot and add the associated serial/lot to the left panel navigation to review its details such as raw material consumption, status, source, and used in serials/lots. If you want to view associated serial/lot details, select the icon from the ACTION column to add the required serial/lot to the queue in the left panel.
    Column Description
    STATUS The status of the serial/lots.
    SERIAL/LOT The target serial/lot identifier that consumed some portion of the selected serial/lot from the left panel.
    MATERIAL The material name, family, and description.
    QUANTITY The initial, current, and used quantities.
    Note:
    The USED quantity is the quantity that was consumed from the selected serial/lot in the left panel by the produced material. However, the INITIAL and CURRENT are the line item quantities of the raw material.

    For example, consider a Bike as a produced material. It has a crankset assembly as a raw material with initial quantity 10. This implies that the current quantity is also 10. Now, when the Bike consumes a crankset assembly, the current quantity of crankset assembly becomes 9.

    Select the crankset assembly in the left panel and then select the Used in tab, you can notice that the USED quantity indicates 1 as the crankset is used or consumed by the Bike (produced material). However, the INITIAL and CURRENT quantity values are that of the line item (individual rows) quantities of the serial/lot and not that of crankset serial/lot.

    LOCATION The location of the serial/lots.
    ACTION
    • : Select to list the details of the respective serial/lot separately. Selecting this creates an entry with the selected serial/lot along with its status color indicator in the left panel.
    Note:
    If you have added a serial/lot to the left panel queue that is a product of a split serial/lot as a result of discrete execution, you can view the BOM consumption tree that indicates the produced material and the produced material consumption records.
  6. Select the Graph tab for a graphical view of the serial/lot relationships of the manufacturing lifecycle. Select a box from the left panel queue, or within a graph, to make it the central item in the graph (surrounded by a blue box outline). Details indicated within the box are:
    • the current status of the item (in the top right corner)
    • the material code of the serial/lot
    • the current location of the serial/lot

    To the left of the selected serial/lot will be a list of the materials, by serial/lot, that were consumed (or nothing if it is a raw material); to the right will be the materials, by serial/lot, that used the selected serial/lot (or nothing if it is the finished product).

    The arrows between the boxes indicate the flow of serials/lots, identifying the quantity and unit of measure.

  7. From the list of entered serial/lots in the left panel, you can use the Enter Serial/Lot search box to search for a specific component from the list.
  8. If you want to remove a specific entry from the left panel queue, select the icon. However, if you want to clear all the entries you made from the left panel, select Clear All.
    Note:
    Any changes (adding/removing/clearing entries) you make to the left panel queue will persist when you navigate away from the Genealogy page.
  9. Select the NCR tab to view the list of non-conformances that are raised on the serial/lot in the Unit Operations or, Work Queue or, Non-Conformance or, Receiving Inspection applications.
    Note:
    For more information on the serial/lot, you can click on View and History icons of that serial/lot in the ACTIONS column.