Disable Discrete Applications
About this task
- Disable the services from the web server
- Hide the applications from the Operations Hub server
Disable the services from the web server
Procedure
- Access the utility.sh in the uc-ansible-installer folder.
-
Provide execution permissions to the utility.sh file by running the following command:
sudo chmod +x /uc-ansible-installer/utility.sh
-
Run the utility.sh by running one of the following commands:
- If you want to run this utility directly on the Web Client node:
/uc-ansible-installer/sudo ./utility.sh -l -disablediscrete reset
- If you want to run this utility remotely on the Web Client node:
/uc-ansible-installer/sudo ./utility.sh -r -disablediscrete reset
- If you want to run this utility directly on the Web Client node:
- If you run this utility remotely, enter the details of the Web Client node.
-
A message appears, asking you to enter Web Client Installation Directory
Enter installation directory and then press Enter.
Hide the apps from Operations Hub
Procedure
-
Access Ophub designer with Ophub tenant user credentials:
https://<ophub-host>/iqp
- Select Plant Applications under Apps.
-
Select NAVIGATION located the top-left corner of the screen.
You need to delete the following Discrete Apps:
- Unit Operations
- Work Order Manager
- Route Editor
- Work Queue
- Time Booking
- Select the app and then select the Delete icon.
-
Repeat the same for all discrete applications.
Now, when you access the Web Client, the Discrete applications are not visible in the left panel.