Configure a Proficy Historian Server for the Analysis Application
About this task
Note:
You can configure a maximum of 10 remote or native Historian
servers in the application.properties file for the Analysis
application.The Analysis application does not
support plotting of Historian tags from Proficy Historian 9.0 version.
Procedure
-
Based on your type of installation, perform one of the following steps:
- Enterprise Installation: In the directory <buildpath>/PlantApplicationsDocker/plantapps-web-docker/mnt/configfiles/historian-config/prod/<version>/, access the historian-config-prod.properties file by using a text editor.
- Standard Installation: In the directory <Installation_directory>\config-repo\historian-config\prod\<version>\, access the historian-config-prod.properties file by using a text editor.
-
In the historian-config-prod.properties file, enter the
properties and their details for each Proficy Historian as described in the following table.
Note:It is recommended to use the same server name format (either IP address, FQDN, or host name) in all the properties to minimize connection issues. For example, if you have entered FQDN for the
hist<n>.service.origin
property, use the FQDN format for thehist<n>.service.hostname
andhist<n>.uaa.origin
properties as well.Property Description hist<n>.service.origin
Enter the IP address, FQDN, or host name of the Proficy Historian server. hist<n>.service.port
Enter the port number on which the Proficy Historian server is installed. Tip:You can leave this property blank if the Proficy Historian server is installed on the default port 8443.hist<n>.service.hostname
Enter the IP address, FQDN, or host name of the Proficy Historian server as configured in Plant Applications Administrator. For example, GESERVER
.Note:The IP address, FQDN, or host name must match with the Server Name configured in the Historian Connections page of Plant Applications Administrator.hist<n>.service.client_id
Enter the client id of the Historian Administrator. - Historian 7.0: admin is the default value.
- Historian 8.0 or later: <hostname>.admin is the default value, where the host name is the server's name where Historian Web-based Clients are installed.
Note:The field for client id is case sensitive.hist<n>.service.client_secret
Enter the client secret of Historian Administrator. Note:The client secret or password must be plain text.hist<n>.uaa.origin
Enter the IP address, FQDN, or host name of the UAA server. hist<n>.uaa.port
Enter the port number on which the UAA server is installed. Note:In the Property column, in each property,<n>
represents a numeric value between 1 and 10 indicating the count of the Historian server configured in the file. For example,hist1.service.origin
,hist2.service.origin
, and so on. - Save changes to the file.
-
Restart the
mes-dataservice-impl-0.6.7
andprocessanalyzer-service-impl-0.6.7
services to apply the changes.