Modify the Value of an Electronic Signature Autolog Variable
About this task
Procedure
- Log in to Plant Applications Web Client.
-
In application navigation menu, select Autolog (Preview)
(
).
-
In the ESIG column, the
icon near the text box indicates that the variable is entitled to electronic signature for any modifications. Modify or enter a new value in the text box for a selected variable that requires electronic signature and then press Tab.
The Electronic Signature window appears. Theicon turns RED indicating that the change in value of the corresponding electronic signature variable. Based on the electronic signature level configured for the variable, the Electronic Signature window appears with the following levels:
- Level-1: Requires only a Performer signature. The Performer Signature section will be available for input.
- Level-2: Requires both the Performer and the Verifier signature. The Verifier Signature section will be available for input after the performer information has been authenticated.
-
If you are a Performer, in the Electronic Signature
window, the following sections and fields are available for you to provide your
performer information.
Field Description Performer Level Stepper indication for an operator or a supervisor to be informed of which level they are into. Indicates the Electronic Signature window is available for inputs of the performer information only.
Note:This indication is display only when both the Performer and Verifier authentication is required.Verifier level This indicator is activated only after the performer authentication is successful and if a verifier signature is required. Note:This indication is display only when both the Performer and Verifier authentication is required.Authenticate Performer Enabled only at the performer level. Select to authenticate through UAA to accomplish electronic signature. After selecting this button, a new tab appears for you to enter the UAA credentials. In the User Account Authentication page, enter the following credentials and then select Authenticate.
- USERNAME: Enter the performer username.
- PASSWORD: Enter the performer password.
Authenticate verifier Disabled at the performer level. This button is activated only if a verifier signature is required. AVAILABLE VERIFIERS Displays the list of available approvers to choose in your vicinity. ADD REASONS Select to expand the section if you want to select a reason. From the available list, select a reason for modification. You can also use the search functionality to select an appropriate reason. ADD COMMENT Select to expand the section if you want to add a comment. You can use this section to add a comment, reason, or note to a verifier about your action. Sign Later This field is disabled. Cancel Select to cancel the changes and revert to the old value. Approve Enabled only after you provide the performer credentials. Select to approve and advance for Verifier authentication. Once you selected this, the verifier level is enabled for the verifier to approve the changes. The Verifier Level is enabled once the performer has supplied the correct performer electronic signature information and selected the Approve option. -
If you are a Verifier, in the Electronic Signature window,
the following sections and fields are available for you to provide your verifier
information.
Field Description Performer Level Indicates the performer credentials has been authenticated and approved. This indicator is disabled at Verifier Level. Note:This indication is display only when both the Performer and Verifier authentication is required.Verifier level This indicator is activated only after the performer authentication is successful and if a verifier signature is required. The Electronic Signature window is available for inputs of the verifier information. Note:This indication is display only when both the Performer and Verifier authentication is required.Authenticate Verifier Enabled only at the verifier level. Select to authenticate through UAA to accomplish electronic signature. After selecting this button, a new tab appears for you to enter the UAA credentials. In the User Account Authentication page, enter the following credentials and then select Authenticate.
- USERNAME: Enter the performer username.
- PASSWORD: Enter the performer password.
AVAILABLE VERIFIERS Displays the list of available approvers to choose in your vicinity. ADD REASONS Select to expand the section if you want to view the reason added by the performer or select a reason from the available list. You can also use the search functionality to select an appropriate reason. ADD COMMENT Select to expand the section if you want to view the comments added by the performer or to add a comment. You can use this section to add a comment, reason, or note to the performer about your action. Reject Select to reject the modifications made by the performer. Once rejected, the modified value is reverted to the old value. You will notice that a new browser window or tab appears and then closes immediately. This is to properly logout the verifier from the browser session. Note:Ensure that the pop-ups are allowed for this web site. You can disable the Pop-up blocker for the web site by adding an exception in your browser settings. When a pop-up is blocked, the address bar will be marked Pop-up blocked.Cancel Select to cancel to log off or unauthenticate. This levels down to the performer level. This helps if you want the performer to make changes to the value based on your suggestion. Once the performer makes the suggested changes, you must again authenticate with verifier credentials and then can approve the changes. You will notice that a new browser window or tab appears and then closes immediately. This is to properly logout the verifier from the browser session. Note:Ensure that the pop-ups are allowed for this web site. You can disable the Pop-up blocker for the web site by adding an exception in your browser settings. When a pop-up is blocked, the address bar will be marked Pop-up blocked.Approve Enabled only after you provide the verifier credentials. Select to approve the modifications made by the performer. You will notice that a new browser window or tab appears and then closes immediately. This is to properly logout the verifier from the browser session. Note:Ensure that the pop-ups are allowed for this web site. You can disable the Pop-up blocker for the web site by adding an exception in your browser settings. When a pop-up is blocked, the address bar will be marked Pop-up blocked.