Add Defects to a Disposition Plan

About this task

If the disposition method and reasons for multiple defects are the same, you can dispose them at the same time. To do so:
  1. Add the defects to a new or existing disposition plan.
  2. Dispose the defects.
You cannot add a defect to a plan if:
  • The defect is created for a non-serialized product.
  • The defect is already added to a plan.

Procedure

  1. Access a non-conformance by performing one of the following tasks:
    • If the non-conformance appears in the workspace or in the left pane, select the link.
    • Enter the non-conformance number in the Search box that appears in the left pane or in the workspace.
    All the defects associated with the non-conformance appear in the workspace.
  2. Select the check box corresponding to each defect that you want to add to a plan.
    Note:
    The check box appears only if the defect is for a serialized product and if the defect is not added to a plan.
    Tip:
    To select all the defects for a non-conformance, select the check box in the heading column.
  3. Select .
    The Create a Plan or add to an existing Plan window appears, displaying a list of plans.
  4. If you want to add the defects to an existing plan, select the plan, and then select Apply.
    The selected defects are added to the plan.
    Tip:
    You can search for an existing plan using the Search box.
  5. If you want to add the defects to a new plan, select Add to a New Plan, and then select Apply.
    A plan is created with a system-generated name, and the selected defects are added to the plan.
  6. Repeat steps 1 through 5 to add defects from other non-conformances to the plan.