Update a BOM Item for a Material Lot

Before you begin

If you do not have the permission to perform this task, request your administrator to provide the permission using Security.

About this task

Use this procedure to update BOM items or custom properties for a material lot.

Procedure

  1. Access the work order whose BOM items you want to edit.
    The page for the work order appears, displaying the Current Status section. The All Serials/Lots section displays a list of serials/lots in the work order, along with the status of each serial/lot.
  2. In the left pane, select the serial/lot for which you want to edit the BOM items.
  3. Select BOM, then under ACTIONS, click Edit BOM Item ().
    A list of BOM items associated with the serial/lot appears.
  4. When updating BOM items, only the following fields are editable:
    • REQ QTY - Value can be set to 0.
    • Custom properties
  5. Click Save to save your changes. To cancel, click Cancel.
    The following rules apply when updating a BOM item:
    • REQ QTY must be greater than or equal to total quantity consumed for the selected BOM item.
    • REQ QTY must be less than or equal to total assigned (issued) quantity allocated for the selected serial/lot number.
    Note:
    You cannot update or add a BOM item when a lot displays an On Hold status. The system displays the following message: BOM changes are not allowed for material lot (Name) due to invalid status (Status Name).
  6. Click Save.