Clock off a Serial/Lot for an Operation

Before you begin

If you do not have the permission to perform this task, request your administrator to provide the permission using Security.

Procedure

  1. In the Unit Operations page, in the Machines box, select the machine that is used to perform the operation.
    The Open workspace appears, displaying a list of operations for the selected machine.
  2. In the row containing the operation for which you want to clock off serials/lots, and then select OFF.
    Note:
    The OFF button is enabled only if you have clocked on the serials/lots in the operation.

Results

The serials/lots are clocked off.
Important:
The Clock on/off button will not appear, if you modify the BEHAVIOR of an operation to Non Clocking in the Attributes tab of a route in the Route Editor application.