Clock on Serials/Lots for an Operation
About this task
Important:
The Clock on/off button
will not appear, if you modify the BEHAVIOR of an operation to
Non Clocking in the Attributes tab of a route in the
Route Editor application.
Before you begin
- If you do not have the permission to perform this task, request your administrator to provide the permission using Security.
- Ensure that the operation is in Ready or In Progress status.
Procedure
- In the Unit Operations page, in the Machines drop-down list box, select a machine.The Open workspace appears.Tip:You can use the USER(S) column to access the IDs of the users who have currently clocked on the operation.
- Select an operation in the Ready or In Progress status.The workspace for the operation appears.
- Optional: Select
to view the details of the operation.
- Optional: If required, update the labor type from the drop-down list box containing the labor types.Note:By default, the default labor type for the operation is selected.
- Select the ON button to enable the clock-on process on the operation.Note:The ON button is enabled only if the operation requires clocking on (as defined in Route Editor or the ERP system).