Post Applications into Operations Hub Manually
About this task
The Plant Applications 2023 Web Client installer can now post the applications into Operations Hub when installing.
When posting applications into Operations Hub fails, you can post them manually.
The OperationsHub_PostingUtility directory within the installer has all the required files. One of the required files is the application.properties file. The application.properties file contains existing basic inputs. However, you must update the below properties in this file:
- opshub.tenant.password=Note:The installer does not support special characters in the password.
- uaa.admin.client.id=
- uaa.admin.client.secret=
Procedure
-
Do the following:
- For Enterprise Web Client, navigate to this directory {{Installer}}/ OpshubPost/.
- For Standard Web Client, navigate to this directory {{Installer}}/ OperationsHub_PostingUtility/.
-
Navigate to the folder, for example, <web client install
folder>\OperationsHub_PostingUtility\application.properties, then
update the application.properties file.
Note:Based on the drive, the default path might change.
-
Run the opshub-posting-utility-1.2.0.jar with the
following command:
java -jar opshub-posting-utility-1.2.0.jar