Set Up the Plant Applications Report Server
Before you begin
- Install the Plant Applications Report (Web) Server.
- In the Services screen, verify that the Plant Applications Report Engine services are logging in under the domain user you specified when installing the Report Server. Check the Log On As column for each service.
- If the Proficy Server Remote Data Service resides on the Plant Applications server, verify that the service logs in under the domain user. If the Proficy Server Remote Data Service resides on another server, such as the Plant Applications Web server, use a Windows user account or a local administrator account with Log on as a Service rights instead of Local System.
- Verify that the domain user has Log on as a Service rights.
Procedure
- Start Excel under the same login account used by the Plant Applications Report Engine services and configure Excel. To get more information on configuring Excel, see Set Up the Plant Applications Excel Add-In.
- Under the Internet Information Services (IIS) Manager, verify that Anonymous Authentication is enabled for the PAReportingFTP site and Rules are added for allowing Anonymous Users to read and write for the three virtual FTP directories (Templates, Reports, and PAReporting). For more details, see Set Up FTP for Report Server.
- Verify that you can use FTP, and log in as
anonymous
. -
Right-click the ..\inetpub\wwwroot folder in Windows
Explorer, select Properties, and then open the
Security tab. Grant full control under Permissions to
all users including
Users
. - In Local Users and Groups (access from Computer Management, or search for “Local Users” from the Windows Start menu), add the following users to the Administrators group:
IIS_IUSRS
(Internet Guest Account)