Install the Plant Applications Server
Before you begin
Verify that you have installed Proficy Application Workflow.
Procedure
-
Copy the software and extract files to the computer where you want to install
the Plant Applications Server, then run InstallFrontEnd.exe
as an administrator.
The Proficy Plant Applications 2023 page appears.
-
From the Installation Menu, under the
Prerequisites group, select Plant
Applications Server. If the installation does not start
automatically, then locate and double-click the
PlantAppsSetup.exe file.
The License Agreement page appears.
-
Select I Agree to accept the agreement.
The Configure Security page appears.
-
Enter the administrator credentials, then select
Next.
You must enter the credentials that you used when installing Workflow, for example, the Proficy (Workflow) SOA Server or Proficy (Workflow) Client.
The RabbitMQ Credentials - MessageBridge Service page appears.
-
Enter the following details, and then select Next.
Credential Description Username Enter the user login name to log into the application during installation. Password Enter the password to log into the application. Confirm Password Reconfirm the password. Note:When you add credentials for a user in RabbitMQ, the system performs the following:- Installs Erlang OTP and RabbitMQ Server.
- Deletes the default RabbitMQ users having "guest" as the username and password, and creates the new user based on above entered user details.
The Install PASP page appears.
-
To install the Plant Applications Service Provider, select the Install Plant Apps Service
Provider checkbox, then select
Next.
Note:The PASP supports Plant Applications versions 4.4.1 and 5.0 for customers using interface methods published with the old version of the service provider. A standalone installation program is available if you install the PASP later. The new MESCore Service Provider, which supports the UMDB, is installed with Plant Applications 6.0 or higher. Methods for the PASP remain documented in the Proficy Workflow help. You must install the PASP to run any workflow applications developed to run against Plant Applications 6.0 and earlier, as they will not run with the new MESCore SP.
The Ready to Install page appears.
-
Select Install to start the installation.
The installation script times out after 10 minutes if the Proficy Server service does not start and prompts you to manually start the service. Once the service is started, the installation automatically continues.
- Verify your installation by checking the installation log files.
Directory Action <Drive>:\<Program Files(x86)>\Proficy\Proficy Server\ Database\SetupLogFiles Verify that VerifyDB and StoredProcedures.log files for the UMDB contain no errors. <Drive>:\<Program Files(x86)>\Proficy\Proficy Server\ Database\SetupLogFiles Verify that its StoredProcedures.log file contains no errors. <Drive>:\<Program Files>\Proficy\Proficy Server\LogFiles Verify that the Plant Applications Service log files, CalculationMgr-xx.log files, and Gateway-xx.log files contain a Connected to Router notification. This notification indicates that the TCP/IP communications are functioning successfully on the Plant Applications Server. <Drive>:\<Program Files>\Proficy\Proficy Server\LogFiles Verify that the Router-xx.log file initialized successfully and does not contain any errors. -
Ensure that you install Plant Applications Report Server after the Plant
Applications Server, but before installing Plant Applications Client. For more
information, see Install the Plant Applications Report Server.
Note:Install Plant Applications Report Server only when reports are required or proceed installing Plant Applications Client. For more information, see Install the Plant Applications Client and Administrator.
-
Install Plant Applications Server SIM, Plant Applications Report Server SIM,
and Plant Applications Client SIM respectively with the latest SIM release
downloaded from the GE Support website. For more information, refer to the
Release Notes of SIMs and read the instructions on SIM KB article
carefully.
Note:Deployment of PADisplayContainer and MESCoreService workflow pf files are done automatically with the Server SIM installer of Plant Applications 2023 SIM7 or later.