Viewing Routes in ECO Hold Status

About this task

When you create a route in the ECO application, the route is in Draft state. After releasing the route, instead of displaying the route in Released state, the route is displayed as "ECO Hold" in the pane under the ECO Hold tab.
Note:
When you enable the ECO Site parameter, the system displays the ECO Hold tab on the Route Editor page.

Procedure

  1. On the Route Editor page, click the ECO Hold tab.
    The View Route page appears.
  2. Verify that all routes released are displayed in the ECO Hold status.
    Note:
    When a route is created in the ECO application and after releasing it, the route goes to the ECO Hold status. In the final approval phase when all approvals are completed, the ECO Hold is released and the route moves to the Released tab.