Viewing Reports

You can view the Reports summary for Product OEE, Order OEE, and Production status as a series of cards based on selected assets.

Procedure

  1. On the Reports screen, select an option from the Show drop-down list.
    • Product OEE
    • Order OEE
    • Production Status
    Show determines the data to be displayed on the cards, such as OEE data or Production Status tracking data.
  2. Select one of the following from the View by drop-down list:
    • Summary (Default option)
    • Department
    • Line
    • Unit
    View by determines the physical assets upon which the display is based, such as Departments, Lines, and Units, with an additional summary view.
  3. You can group the information as per your requirement
    View by optionGrouping options
    Summary (default option) or DepartmentGroup by drop-down-list contains the following options:
    • None (default option)
    • Shift
    • Crew
    LineIn drop-down list contains a full list of department names. Example:
    • Department 1
    • Department 2
    • Department 3
    You can also group results by none, shift, or crew.
    UnitIn drop-down list contains a full list of line names. Example:
    • Line 1
    • Line 2
    • Line 3

    You can also group results by none, shift, crew, or path.

  4. Select the required time range and click the refresh button next to the drop-down to view and update the results.
    • Current Shift (Default)
    • Last Shift
    • Today
    • Yesterday
    • Current week
    • Last week
    • Custom
    • Tomorrow (for Production Status only)
    • Next Week (for Production Status only)
    • Next Shift (for Production Status only)
    The time range that you select will be displayed in the form of date and time next to the time-interval drop-down list. The Reports screen generates the report for the selected options. For example, if you select Product OEE by Line in department 1 grouped by Shift for the current shift, the application generates a list with the following information:
    • A summary of KPIs is displayed at the top: OEE, Quality, Performance, and Availability
      Note:
      The KPI values are based on the selected time range and not on the Product or Order time durations.
    • For each line, grouped by shift, following columns are displayed:
      • Product – Products produced on the Machine or Machine group. If the report selected is Product OEE, this column shows the Product information. If the report selected is Order OEE, this column shows the Order information.
      • Status – When an OEE exceeds an established threshold, the Status column displays a red dot.
      • Separate columns display each KPI for the listed products: OEE %, Performance %, Availability %, and Quality %.
      • The last row for each shift displays the Total value rolled up for each KPI card.
    If you select Production Status in the Show drop-down list, you see the production status report for the model context selected through View By and In drop-down list and grouped by the Group by category. The report view includes the following information:
    • Order (sortable) – The list of Orders in the Machine or Machine Group, or as a Summary, as per the orders configured in the Plant during the time range selection made.
    • Product – Name of the Product associated with the Order in the row.
    • Status – the status of the Order (for example: Completed, Active, Pending).
    • Complete % – completion percentage at the time the Report is displayed.
    • Start – start time of the Order. If the Order has already started or completed, this time shows the actual time, else it displays the planned time.
    • End – End time of the Order. If the Order is already completed, this time shows the actual time, else it displays the planned time. If the order is in process, it displays the estimated time.
    • In-line View – If you select a row, an in-line view opens, displaying Production Information along with the Planned vs. Actual values of Quality and Schedule.
  5. Optional: Click a row to see the color chips for all the three KPIs. The colors of these chips indicate the ranges of the KPI values which are static and are not based on Product or plant model context.
  6. Optional: Click a row to see the details of the KPIs of that particular row.
    The row expands to display Planned vs. Actual raw values of the KPIs for the corresponding row.
  7. Optional: For any combination of the Options selected, once the data is retrieved and displayed they can be exported to a csv file by clicking the export icon on the right top corner of the cards.